This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIL313 Old 7-Segment Display Datasheet

Anonymous
Anonymous

I have an old 7-segment display from a game I took apart and it is clearly a Texas Instruments part but I entered the part number (TIL313) in the search box to see if anything would come up but nothing did.  I was wondering if anyone had a datasheet that would helpful.  It is a red 0.30" display in a 14 or 16 pin 0.3" DIP format with 8 or 10 pins centered between the two ends on each side of the package.   Thanks for any help you can give me!