Part Number: DP83867IR
Hi team,
I have a question about PHYCR.
According to page 67 on the datasheet(SNLS484E), bit[6:5] in PHYCR is
listed as RO.
I understand those bits are RW.
Is my understanding wrong?
Sincerely,
Tsuyoshi Tokumoto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83867IR
Hi team,
I have a question about PHYCR.
According to page 67 on the datasheet(SNLS484E), bit[6:5] in PHYCR is
listed as RO.
I understand those bits are RW.
Is my understanding wrong?
Sincerely,
Tsuyoshi Tokumoto
Hi Geet-san,
Thank you very much for your prompt reply.
Please let me ask you two additional questions.
Q1)Can the DP83867IRPAPR be configured to 10Mbps(fixed) or 100Mbps(fixed) with
Disable Auto-Negotiation by using Strap pins?
Q2)If the device set to the following values by the Strap pins is
turned on,will the port speed be set 1000Mbps?
AGEN_SEL[1:0]=b'11
Autoneg Disable=b'1
Thank you and best regards,
Tsuyoshi Tokumoto
Hi Tokumoto-san,
Q1: ANEG_SEL[0:1] = 11 shall help force the link to 10/100M speed.
Q2: For 1000M, ANEG_SEL[0:1] : 01.
Regards,
Geet
Hi Geet-san,
Thank you very much for your prompt reply.
Please let me ask you two basic questions.
I am being asked from my customer about the port speed
when Auto-Negotiation function is disabled through the straps.
I found out a following post on E2E.
According to the above post,I understand that the PHY cannot be forced
into any speed through straps and the speed select straps are used for controlling
auto-negotiation advertisement.
From the above,
Q1) I think that the port speed is configured to 1Gbps immediately after the power-on,
because the default values of bit6 and bit13 of BMCR are set to b'10.
Is my understanding correct?
Q2) If a user want to fix the port speed,the user will have to write the configuration
values directly to bit6,13 of BMCR through the MDIO/MDC.
Then, the user will have to perform the global-software-restart(setting bit 14 of register
CTRL to 1).
Is my understanding correct?
In addition, will there be anything that the user should be careful of?
Thank you and best regards,
Tsuyoshi Tokumoto
Hi Geet-san,
I am still expecting your response regarding my questions.
Thank you and best regards,
Tsuyoshi Tokumoto
Hi Geet-san,
Thank you for your reply and I apologize for the delay
in replying to you.
My questions have been almost cleared up, but please let me reconfirm
the following question.
When my customer wants to use force mode(Auto-Neg disable)
and use 100M speed, performing the global-software-restart(setting bit 14 of register
CTRL to 1) is needed after writing "01" to bit6,13 of BMCR through the MDIO/MDC.
Is my understanding correct?
Thank you and best regards,
Tsuyoshi Tokumoto
Hi Pimentel-san,
Thank you very much for your reply.
My questions have been cleared up!
Thank you and best regards,
Tsuyoshi Tokumoto