Part Number: DS125DF111
Hi Team,
Is polarity allowed for both input and output?
is allowed only for output?
Thanks
Arunkumar K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS125DF111
Hi Team,
Is polarity allowed for both input and output?
is allowed only for output?
Thanks
Arunkumar K
Hi Michael,
I am asking *_P and *_N can be swap-able or not?
in datasheet it is mentioned that only output is possible. am i right?
If i am changing the concern register value will it change the output of both the channel?
Arun
Hi Arun,
Yes, through register control for each channel, you can invert the polarity of the output. This is intended for the purpose of trace-routing simplicity.
These settings can be controlled individually. In Reg 0xFF, first define which Channel you wish to control, then the value of Reg 0x1F[7] will correspond to the behavior of that channel's driver polarity.
Regards,
Michael