Part Number: ISO5851-Q1
Other Parts Discussed in Thread: ISO5851
Hi,
I would like to use the ISO5851-Q1 to control an IGBT on a 800V line with just a heating resistance on it.
In case of CC of the resistance, I want to use the DESAT function to open the line.
But I can't find in the datasheet the dimensioning of the DESAT funciton, in particular the Ddesat: must this one have a reverse voltage of 800V in my application ?
Thanks in advance,
M. NEDELEC