Part Number: USB-2-MDIO
Other Parts Discussed in Thread: MSP430F5529
In 
Was said "We can share though a pseudo code and basic process for implementation if that would help you in your development.". How can I get it? It would be great to have a possibility to have a python script able to read and write into the PHY using the MSP430F5 launch pad. To make that it would be ok to have better understanding of the commands that USB-2-MDIO send over the com port to init (connect / select extended addressing etc), and the read an write registers. Another option would be to have command line options in the USB-2-MDIO tool to instruct it to connect / read and write. That would allow to use the USB-2-MDIO tool from python to read and write.