Part Number: DP83867E
Section 8.4.5 of the datasheet states "The BIST allows full control of the packet lengths and of the IPG." I can find a bit field PACKET_GEN_64BIT_MODE in BIST Control Register (BISCR) which offers at least some (not full..) control of the packet lengths, but which register allows (full) control of the IPG?