Part Number: DS90UB928Q-Q1
[ DS90UB928-Q1 ] Video Output Disrupted during ESD Testing
Hi,
My customer has reported that their display image is disrupted during ESD testing.
When they hit the ESD pulse as conditions below, video image is disrupted for a while and back to normal operation.
(Whole system still remains normal operation. Not occured everytime like 3 times per 10 pulse shot.)
----
ESD Pulse Condition
---
- Indirect Discharge: +/-4.6kV
- Direct Discharge: 4kV
(Charge/Discharge capacitance: 2kohm/330pF)
---
Customer has tried several things such as adding small caps (0.1uF, 0.01uF) for VDDxx pins. But does not make any improvement.
Do you have any ideas to improve this behavior?
I would suggest customer to add additional small caps onto CAPxx to robust the output noise perfromance from internal voltage regulator.
How do you think?
Thank you for your support in advance.
Regards,
Ken