Part Number: LMH1983
Dear Team,
Please see below questions from my customer :
- Operation on Holdover mode:
“When locked to reference, an internal 10-bit ADC will track the loop filter control voltage.
When a loss of reference (LOR) occurs, the LMH1983 can be programmed to hold the control voltage to maintain output accuracy within ±0.5 ppm (typical) of the previous reference.
The LMH1983 can be configured to re-synchronize to a previous reference with glitch-less operation.”
For what period of time could the Holdover synchronization be kept (what is the deviation rate from the original reference)? - Scenario of wrong input format and transition to Free-run mode:
In case the input format (Hin, Vin) is not recognized by the LMH1983 as a known\legit format right from the start/power-up.
The reference was never locked and the LOR mode (register 0x05 bit 2) is set to its default value (0= Holdover on LOR).
Will in this case the LMH be transiting to a Free-Run mode (though it is configured to a holdover on LOR)?
Best regards,
Nir