This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9539: Writing to only one Output Port

Part Number: TCA9539

Figure 31 on page 24 of the TCA9539PWR datasheet shows data being written to both Output Port 0 and Output Port 1 in the same I2C operation.

My question is, can I write to only Output Port 0 without writing to Output Port 1 (i.e. issue a stop command after the first byte of data)? Or am I forced to write to both output ports?

  • Hey Ro,

    "My question is, can I write to only Output Port 0 without writing to Output Port 1 (i.e. issue a stop command after the first byte of data)?"

    -Yes, you can stop sending data after the first byte. (Writing to Output Port1 is not required)

    "Or am I forced to write to both output ports?"

    -Not required.

    Figure 31 is meant to show that this device has an AI (auto increment) feature which works in register pairs (input|output|configuration|polarity) and is important for the designer/user to understand it is there.

    Thanks,

    -Bobby

  • Thanks, Bobby!