Part Number: DP83822I
Hello, i am using the dp83822 configured to operate in RMII slave 50Mhz interface mode.
Enabling the MII lopback (BMCR register, bit 14, all other BMCR bits clear), I have no data returned on the RMII RX while sending on RMII TX.
Is the MII loopback only working with a MII interface only and I need to use a PCS input loopback instead ?
Thxs
Pascal