Part Number: TUSB546EVM
Other Parts Discussed in Thread: TPS65982, DP-EXPANSION-EVM, TPS65981
I'm testing with TUSB546EVM board, and the IC used in the project is TUSB1046 and TPS65982.
This project converts DP video source to USB Type-C, and it is a device to check video source by
connecting to a mointor that supports USB Type-C.
When the monitor and the device are connected, I have a question about the external voltage setting from the
monitor to the device.
1. TPS65982 flash is the same as EVM.
2. The device always inputs 5V.
3. Is there any way to change the voltage input from the monitor to the device to 5 ~ 20V?
Thanks.