This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: I want to know the difference between DS90UB964 and DS90UB960

Part Number: DS90UB960-Q1

   Dear all:

        I want used DS90UB960,but it not release. Is it the same as DS90UB964 except resolution? Can we used DS90UB960 replace DS90UB964 if it release? thanks

  • Hello,
    The DS90UB960 supports 2MP+ resolution typically and 1080p/60fps imagers vs 1MP+ and 720p/60fps or 1080p/30fps imagers for the 964. Also the 960 supports synchronous clocking mode (when used with 953) and provides some advanced diagnostic features compared to the 964.

    For additional information on the 960, you can contact your local TI sales/field representative.
  • Dear  Palaniappan:

         Thanks for your support ! I have a problem about DS90UB960.

         If we used DS90UB953, we need used DS90UB960 as DES HUB?   DS90UB964 not support DS90UB953? only support DS90UB913A/933?

  • Hello,
    The 953 serializer can work with 914A and 934 deserializers in the backwards compatible mode with parallel outputs, but for the CSI-2 mode you need to use the 960 with the 953. The 964 version supports 913A/933 serializers only.

    Also as mentioned before the 960 has some additional features such as synchronous clocking mode when used with the 953.