Part Number: DS90UB964-Q1
Other Parts Discussed in Thread: DS90UB913A-Q1
[ DS90UB964-Q1 ] CSI-2 Transmitter Frequency Calculation
Hi,
Can you please help me to figure out the CSI-2 Transmitter Frequency?
From the reference post below, is this valid estimation?
[ Horizontal Pixel Count ] x [ Vertical Pixel Count ] x [ Frame Rate ] x [ bit width ] = CSI-2 Transmitter Data Rate
So, if I use same example as reference post,
1280 x 720 x 30 x 12 = 331.776Mbps
Thus, 400Mbps or 800Mbps setting can support this.
My customer would use much higher resolution with RAW10 mode such as a equation below.
3000 x 1000 x 30 x 10 = 900Mbps
So for this case, customer need to use 1.6Gbps or 1.472Gbps mode.
Is this estimation correct?
Thanks,
Ken
DS90UB964-Q1: CSI-2 TX Frequency
e2e.ti.com/.../623778