Part Number: DS90UB964-Q1
[ DS90UB964-Q1 ] RAW10 8-bit mode
Hi,
Can you elaborate the RAW10_8BIT_CTL register bit (0x7C[7:6]) in the PORT_CONFIG (0x7C)?
Even though we use this RAW10 8-bit mode (either 10 or 11), CSI data type still need to be set as RAW10 (Not RAW8). Correct?
(CSI data type specifies RAW8 data type as well)
My customer would use DS90UB964-Q1 in conjunction with four DS90UB913A-Q1s with RAW10 mode.
But actual data bit is 8bit out of 10bit, thus it may be required to configure this bit.
Thanks,
Ken