Part Number: SN75176B
Other Parts Discussed in Thread: TIDA-00527
Hi Folks,
First of all, sorry, if this is not the right forum for my question.
I have to plan a system / solution, where I have to generate PWM signals occasionally far from each other (~50m), but due to cost consideration, placing a CPU to everywhere is not an option. So I wanted to transmit my PWM signals trough differential lines, on the same wire where the power goes for the receiver chip. I fond the TIDA-00527 reference design.
So my question is: what should I modify (which jumper path should I select) to transmit PWM signals around 2kHz with DutyCycle 1-99% and 12-24V on the same wire? Even somebody know alternative / cheaper / better solution?
Regards,
Norbert