This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DP130: Internal pull up resistor variation for RSTN pin.

Guru 19785 points

Part Number: SN75DP130

Hi Team,

Please allow me to ask you about the internal pull up for RSTN pin.

User is required to release reset after more than 100us from Vcc/Vdd are stable.

When RSTN is controlled with external cap, we need to calculate the capacitance to meet above requirement.

In this case we need to know the following 2 information.

1). What is the internal pull up resistor variation ? Rrstn=150k Ohm (TYP). What is MIN and MAX ?

2). When used in single supply mode, what is the MIN and MAX spec for the regulated Vddd output ?

Best Regards,

Kawai