Part Number: TUSB4020BI
Other Parts Discussed in Thread: TPS2540, TPS2546, TPS2561
I have the 4020 in AutoMode, battery Charge enabled, fullpwrmgmnt enabled, Ganged OFF, ILim of 2561 ~ 1.25 A. Everything works as expected except an over current event doesn't result in the port being disabled. I monitor the OVERCUR1Z from the 2561 and it goes low but the enable from the TUSB never transitions.
EEPROM code
00 55 01010101
01 51 01010001
02 04 00000100
03 40 01000000
04 84 10000100
05 10 00010000 'ganged off, over current on
06 0F 00001111 'bat chg on for both ports
07 0C 00001111 'ports removable
08 0F 00001111
09 00 00000000
0A 70 01110000 'auto mode on, high I div mode off
0B 00 00000000
0C 00 00000000
0D 00 00000000
0E 00 00000000
0F 00 00000000
10 00 00000000
11 00 00000000
12 44 01000100
13 84 10000100
14 05 00000101
15 84 10000100
16 EA 11101010
17 35 00110101
18 09 00001001
19 16 00010110
1A 86 10000110
1B 78 01111000
1C AE 10101110
1D C9 11001001
1E D0 11010000
1F 00 00000000
20 09 00001001
21 04 00000100
22 00 00000000
23 00 00000000
24 00 00000000
25 00 00000000
26 30 00110000
27 00 00000000
28 00 00000000
29 00 00000000
2A 00 00000000
2B 80 10000000
2C 00 00000000
2D 00 00000000
2E 00 00000000
2F 00 00000000
30 32 00110010
31 00 00000000
32 30 00110000
33 00 00000000
34 30 00110000
35 00 00000000
36 30 00110000
37 00 00000000
38 30 00110000
39 00 00000000
3A 38 00111000
3B 00 00000000
3C 34 00110100
3D 00 00000000
3E 31 00110001
3F 00 00000000
40 42 01000010
41 00 00000000
42 41 01000001
43 00 00000000
44 41 01000001
45 00 00000000
46 33 00110011