Part Number: SN75DP130
Hi
I want to design using SN75DP130 in sink side.
[DP Connector (Source)] ----> [SN75DP130 Re-driver] --------> [ FPGA]
I has some questions
1. Datasheet has only source side guide. Do you have some reference schematic of sink side?
2. FPGA need AC cap in AUXSNK line like below. Can I put the AC cap in AUXSNK line?
[SN75DP130 Re-driver AUXSNK] ------> [AC CAP] --------> [ FPGA]
3.Refer to below image.
When I using as Sink side re-driver, AUX_SRCP/N, SCL_DDC and CAD_SRC is must be unconnected like below guide?