Hi Team,
I need urgent help please with TPS65986.
The chip was flashed with a bin file I’ve got from configuration application. Flash load occurs OK, as far as I can see from constantly switching CC1 and CC2 signals.
The problem is that the chip does not answer to I2C. (it shares I2C with charger, fuel gauge and LED driver, they work OK, no address conflict as well, but TPS65986 always returns NACK from the first address write, I tried 0x38, 0x70, 0x20, 0x40 as an address, just NACK and that’s all). The I2C_ADDR pin is hardwired to GND. The configuration application displays 0x38 as an address. The sleep is configured so that TPS65986 can miss first transaction, so I make dummy transaction of 1byte address write. I get NACK in both first dummy and second real transaction.
Could You please help me understand what can it be?
Thanks a lot and Best Regards,
Shlomi