This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: Regarding RJ45 connector with built-in tolerance

Part Number: DP83867IR
Other Parts Discussed in Thread: DP83867E

I have a question.

Is it possible to use Pulse Electronics [JK 0654219 NL] of RJ45 connector with built-in transformer?

==============================


The specifications of the connector are described below.

· TURNS RATIO
         1: 1 ± 2%

· INSERTION LOSS
         -1.2 dB MAX (100 kHz)
         -0.2 - 0.002 * f ^ 1.4 dB MAX (1 - 125 MHz)

· RETURN LOSS (Z OUT = 100 Ω ± 15%)
         -16 dB MIN (0.1 - 40 MHZ)
         -10 + 20 * LOG (f / 80 MHz) dB MIN (40 - 100 MHz)

· INDUCTANCE (OCL) * MEDIA SIDE, 0 ° C - 70 ° C)
         350 uH MIN (MEASURED AT 100 kHz, 100 mV RMS AND WITH 8 mA DC BIAS)

· CROSSTALK, ADJACENT CHANNELS
         -50 dB MIN (1 MHz)
         -55 + 22 * LOG (f / 10) dB MIN (10 - 100 MHz)

· COMMON MODE REJECTION RATIO
         -50 dB MIN (2 MHz)
         -15 + 20 * LOG (f / 200) dB MIN (30 - 200 MHz)

· DC REDIDTANCE, 1/2 WINDING "
         0.65 Ω MAX

· DC REDIDTANCE IMBALANCE
         ± 0.065 Ω MAX (CENTER TAP SYMMETRY)

· INPUT - OUTPUT ISOLATION
         2250 VDC MINIMUM FOR 60 SECONDS

JK0654219NL.pdfJK0654219 Test Note Dec 2016.pdf

==========================

Best regards

ozawa

  • Hi Ozawa-san,

    It is recommended to use a magnetic that meets the electrical specs of the transformer on the DP83867E EVM.

    That transformer is the Pulse HX5008FNL.

    In the spec you posted, the -1.2dB insertion loss is not recommended for the DP83867.

    Best Regards,