Part Number: DS90UB940-Q1
Hi,TI,
I'd like to confirm the I2S clock of Ds90UB940. could you please answer the questions ?
Q1. Is it possible to use the I2S clock at 705.6KHz ?
Q2. In the "8.3.12.2 I2S Jitter Cleaning" in the data sheet, It mentioned that
.... less than 1MHz, this feature must be disabled through register 0x2B[7]......
But the add:0x2b[7] was reserved and there is no description in the data sheet.
In order to bypass the jitter cleaner, user should set 1 to the 0x2b[7], correcgt ?