Part Number: TIC12400-Q1
Hi,
I designing some device into aircraft and this part looks very usable for us, but I need know answers for several questions.
1. Can you tell me what is maximum working altitude for this part?
2. if it is know, is there (if any) temperature derating when I use it for measure inputs up to 34V? The power supply can be lower if it is needed for some reasons.
3. if it is know, is there (if any) temperature derating when the power supply will be 27V (up to33V)?
Thank you for answers.
Miroslav Pajpach