Part Number: SN65HVD75
Other Parts Discussed in Thread: THVD1550
Hi.
We need to design a RS485 interface with baud rate 921600 bps. We plan to use the SN65HVD75 tranceiver.
CPU that will be used supports x8 and x16 oversampling at this speed on its UART interface. We can cover the x8 oversampling with single oscillator, but need additional for the x16, so the x8 oversampling is preffered. I would like to find out if x8 oversampling is reliable enough. The clock mismatch error is 0.16%. Max number of units on the bus is 32. We are slave on the bus. The masters we will need to work with are unknown at this moment, conditions on the RS-485 bus are unknown also.
Can you provide any insights into x8 vs x16 oversampling dilemma?
Thank you and best regards,
Borut Cadez