Part Number: TPS25810
Hi Sirs,
As title, we finished 25810 schematic (U188).
Our Type C connector only had USB2.0 function and CC pin.
Could you help double confirm our schematic again?
Thanks!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS25810
Hi Sirs,
As title, we finished 25810 schematic (U188).
Our Type C connector only had USB2.0 function and CC pin.
Could you help double confirm our schematic again?
Thanks!!
Hi Sirs,
Thanks for your reply.
The schematic looks good. I would change C2462 to 6.8uF
Because we don't have 6.8uF internal, the 4.7u will too small??
For testing purposes you may want to add a pull-up resistor on the fault pin just to know if the TPS25810 is faulting or not.
Is it OK if we only reserved 4.7k resistor?? or really need put on this resistor to the board??
Hi Shu-Cheng,
4.7uF should be ok.
You do not have to put the pull-up resistor on the board if space is limited but it may be helpful when testing the board.
Regards,
Donovan