Part Number: TUSB320LAI
Other Parts Discussed in Thread: HD3SS3220
If the OUT1\2 pins are configured for GPIO what is the recommended value for the pull up resistors ?
The only value give is 4.7K but that is for I2C.
The value for the External pullup resistor on open drain IOs (INT_N/OUT3,ID) : 200K - but OUT1/2 is not mentioned ?
OUT1\2 when it is configured as an GPIO is also defined as an open drain in the data sheet ?
Also for the HD3SS3220 the External Pull up resistor on Open Drain IOs (OUT1, OUT2, INT/OUT3) : 200K