This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/SN65HVD255: SN65HVD255 IBIS Model

Part Number: SN65HVD255

Tool/software: WEBENCH® Design Tools

Hi team,

My customer is meeting a problem that IBIS model of SN65HVD255 isn't convergent.

I have uploaded their simulation file, could you please kindly help to check out the reason?

Thanks!

**** Tlsim Version 16.2 ****

**** Tlsim command line ****
 tlsim -r 0.050000 -BhvrSplineOn -o waveforms.sim -dl delay.dl -dst distortion.dst -log tlsim.log -ocycle cycle.msm main.spc


Number of Nodes in this circuit = 173


Statistics on N-line elements:
 Number of 'n' type multi-conductor elements = 17
 Type-of-N-element  #elms Max_Length TotalLength

 2-line-N-elm     17   0.508    3.8862
 Total Interconnect Length = 7.7724
 Total Coupled Length = 7.7724

 Following is some statistics on Model usage
   Model-Type      Model-Name     Number-of-Models-in-this-circuit

   bdrvr         HVD255_CANL_BI_Typ_27degC               2 
   bdrvr         HVD255_CANH_BI_Typ_27degC               2 
   bdrvr         AMIS30660_CANL_BI_Typ_27degC               6 
   bdrvr         AMIS30660_CANH_BI_Typ_27degC               6 
  No of 'Bdrvr' type model instance = 16

 Time Step at Start = 5e-011



 Simulation will start at t=0 and end at t=4.00719e-006. 


*********************************************
*  WARNING: Convergence Problem detected    *
*********************************************
Solution did not converge during transient analysis
No of iterations = 41 
 Time = 1e-010 
 Max Residue = 0.983797 
		Matrix Size = 10

*** ABORT: Transient Convergence Problem Is Severe ***

*** Suggested solutions are ... ***

*** Since you have bhvr models try the switch '-BhvrTransientModifyNewtonOff' ***

*** try using resistors(large) to ground and/or capacitors between nodes to filterout high freq noise***


*** Examine circuit attached to  Node 'DESIGN.SLOT6.7' ***
*** other nodes in this circuit are -- ***
 '24464RL' 
 'DESIGN.SLOT6.7i' 
 'DESIGN.SLOT6.7i_DESIGN.SLOT6.6i_comm' 
 'DESIGN.SLOT6.6i' 
 '26962RL' 
 'DESIGN.SLOT6.6' 
 'DESIGN.SLOT6.7_DESIGN.SLOT6.6_comm' 

**** Transient Simulation Statistics ****

    Number Of time step solutions = 2

**** Tlsim Run Times ****

    Start time = Mon Jan 15 15:22:25 2018

    Finish time = Mon Jan 15 15:22:25 2018

    Elapsed time = 0 hours, 0 minutes, and 0 seconds

  • Susan,
    We're working with webench team for debug. We will get back to you shortly.
    Regards,
    Hao
  • Susan,

    We used HyperLynx to run IBIS model and didn't see any issue.

    Can you check what software your customer used? And how they set up the bench? Thanks!

  • Hi Hao,

    Thanks to your answer.

    The software my customer used is Sigxp.

    I have uploaded their simulation error Log, please kindly help to check the error. Any specific information needed, feel free to let me know.

    Thank you ! 

    **** Tlsim Version 16.2 ****
    
    **** Tlsim command line ****
     tlsim -r 0.050000 -BhvrSplineOn -o waveforms.sim -dl delay.dl -dst distortion.dst -log tlsim.log -ocycle cycle.msm main.spc
    
    
    Number of Nodes in this circuit = 197
    
    
    Statistics on N-line elements:
     Number of 'n' type multi-conductor elements = 17
     Type-of-N-element  #elms Max_Length TotalLength
    
     2-line-N-elm     17   0.3683    3.302
     Total Interconnect Length = 6.604
     Total Coupled Length = 6.604
    
     Following is some statistics on Model usage
       Model-Type      Model-Name     Number-of-Models-in-this-circuit
    
       bdrvr         HVD255_CANL_BI_Typ_27degC               1 
       bdrvr         HVD255_CANH_BI_Typ_27degC               1 
       bdrvr         AMIS30660_CANL_BI_Typ_27degC               7 
       bdrvr         AMIS30660_CANH_BI_Typ_27degC               7 
      No of 'Bdrvr' type model instance = 16
    
     Time Step at Start = 5e-011
    
    
    
     Simulation will start at t=0 and end at t=4.0067e-006. 
    
    
    *********************************************
    *  WARNING: Convergence Problem detected    *
    *********************************************
    Solution did not converge during transient analysis
    No of iterations = 41 
     Time = 1e-010 
     Max Residue = 1.10611 
    		Matrix Size = 11
    
    *** ABORT: Transient Convergence Problem Is Severe ***
    
    *** Suggested solutions are ... ***
    
    *** Since you have bhvr models try the switch '-BhvrTransientModifyNewtonOff' ***
    
    *** try using resistors(large) to ground and/or capacitors between nodes to filterout high freq noise***
    
    
    *** Examine circuit attached to  Node 'DESIGN.SLOT0.7' ***
    *** other nodes in this circuit are -- ***
     '24' 
     'DESIGN.SLOT0.6' 
     '23281RL' 
     'DESIGN.SLOT0.6i' 
     'DESIGN.SLOT0.7i_DESIGN.SLOT0.6i_comm' 
     'DESIGN.SLOT0.7i' 
     '16827RL' 
     'DESIGN.SLOT0.7_DESIGN.SLOT0.6_comm' 
    
    **** Transient Simulation Statistics ****
    
        Number Of time step solutions = 2
    
    **** Tlsim Run Times ****
    
        Start time = Tue Jan 30 12:03:23 2018
    
        Finish time = Tue Jan 30 12:03:23 2018
    
        Elapsed time = 0 hours, 0 minutes, and 0 seconds

     

  • Susan,

    Unfortunately I'm not familiar with this tool. But after reviewing the log, it looks like this is more like a setup issue. Can you get more information about the simulation setup? Here is mine for your reference.

    They can also try the two suggestions the tools gave: 1) try the switch '-BhvrTransientModifyNewtonOff'; 2) adding big resistors to ground and cap between nodes. Usually it's not helpful to leave any node undefined in the simulator.

    Regards,

    Hao