Other Parts Discussed in Thread: TPS65982, , TPS65982-EVM
Hi Ti Team,
I have a question to the dead battery mode of the TPS65981.
As I read in the datasheet, it is possbile to operate the device with VBUS only, without 3.3V on VIN_3V3. The TPS65981 then goes into dead battery mode. By selecting the right voltage on BUSPOWERZ I can choose the external power path to sink to my further system. My application is only in sink-mode, so I think the TPS65981 can stay in dead battery operation or is there any problem?
Thanks for your help.
Regards
Dimitri Schmidt