Part Number: TPS2062
Other Parts Discussed in Thread: TPS2061
Hi,
PLease support to provide your comments for questions as below.
1. What is the Vih and Vil for EN1 and EN2 pins? Considering to disable the switch by connecting ENx pins to 3.3V, is it necessary to add any PU resistor? Or PD resistor when it's connecting to GND to enable the switch?
2. When there's no loading on Out1/Out2(No USB device connected) with ENx high( to disable output) by default during system power-up, what would be the the output voltage level at this moment?
3. Is there any power on sequence requirement for IN/ENx/OCx pins?
4. What would be the suggested way to connect ENx pins when we want to keep this switch disabled (so that output is 0V) during system power-up?
Antony