Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS80PCI402: Relation for priority the register and RATE pin setting

Guru 19685 points

Part Number: DS80PCI402

Please let me know about four points below for priority the register setting and RATE pin setting(Gen 1~3);

①RATE pin setting is more priority than register default setting, is it correct?

②Once register set by SMBus, is DS80PCI402 move according to not RATE pin but SMBus register setting?

③If above are correct, I think that setting priority is "Default setting < RATE pin setting < SMBus setting", is it correct?

④If DS80PCI402 setting is always used SMBus, is RATE pin setting anything OK? (VDD, GND, Floating, etc) 

Best regards,

Satoshi

  • Hi Satoshi-san,

    1. Yes the RATE pin has a higher priority against the register defaults.

    2. In order to switch the priority and make SMBus > RATE pin the application must write the override bit in Register 0x08.  Then the SMBus setting will take priority.

    3. See #2

    4. If the plan is too use SMBus override to control RATE, I would recommend to set the configuration pin RATE = Float.

    Regards,

    Lee