Part Number: THVD1510
Hello Team
I have some question about the RE/DE enable time
1) general when 485 chip, we connect RE and DE together. But they have difference enable time, please see the following data. When the part change from Receiver to Driver, the time RE from VCC to 0V will need 500ns, but DE from 0v to VCC will need 8us. So which time will detemine the last change.
2, if the two pin separate control, both of them are enable. can the RXD receive TXD data?