Dears,
May I ask two questions about DP83822IRHBR? Thank you .
My customer uses this config as belows (the red rectangle):
My question is :
1/ If I don't insert the internet cable , can I get the FLP signal ? Actually , I can't get the FLP signal in Oscilloscope.
I'm not sure if the DP83822 will always generate the FLP signal in this config mode.
2/ We set the Auto-Negotiation enabled by regsiter configuration, using bit[12] in the Basic Mode Control Register (BMCR, address 0x0000).
When inserted the internet cable, DP83822 maybe works in 10base, mybe works in 100base. What is the major factor to determine DP83822 work speed? 10base or 100base?
Thank you very much.