Part Number: DS90UB954-Q1
Dear Sir/Madam,
I am facing strange issue when connect my image sensors to 953 via 954 before display on the screen. Below is the test steps:
1. without image sensors, if I use the internal test pattern and output to 954, the test pattern is able to display correctly on the LCD display, something similar like below:
2. However, if I connect the my image sensor to the 953 and output via 954, I get the following output pattern distortion. The image distortion always happened at the same location. (please ignored the water mark behind the second line)
the white and black pattern are correct, only the test pattern in between white and black is having issue after it display correctly at beginning portion.
I don't think it is the hardware issue since the test pattern without image sensor is able to display correctly in step1.
Any expert can advise what could be the issue?
Best regards,
kpk