This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Data wanted for Plasma display drivers SN755870 and SN755881

I am after data for Plasma display drivers SN755870 and SN755881.

These chips are readily available (as spares for Plasma TV displays) and are shift-register with high voltage outputs.

These have outputs that can drive about 200v and run off 5v logic (unlike the Supertex parts which require level-shifters as they need 12v)

All the older datasheets seem to have disappeared from Ti site (another plasma driver was SN751518 which is unfortunately an unavailable part but did have a datasheet until recently)

Can someone help or suggest where I can find data on SN755870 and SN75588 ?

Thanks,

Andrew