Part Number: DP83867IR
Hello .
I am facing interface issue with DP83867IRPAP PHY device.
Problem statement: Unable to establish link between this device and switch (moxa :EDSG205-1GTXSFP-T & D-Link : DGS-3100-24).
Observation:
1) PHY is configured for MII 100 BASE-TX_Full Duplex mode.
2) PHY interface of 100Mbps with PC is successful.
3) PHY interface with MOXA & D-Link switch is not able to estabelish a link.
4) Fast Link Pulses are present at Physical Layer of both end i.e. PHY as well as MOXA-swicth/D-Link Switch:
5) As per Clause 28 of Auto Negotiation
a) PHY FLP decoding is : 1000 0111 1000 0000
b) MOXA-swicth FLP decoding is : 1000 0111 1011 0001
I am attaching the circuit for reference . PHY_Schematic.pdf
please do the needful to resolve the problem .
Regards
Daman