Part Number: TCA9509
Hi team,
I am planning to build a board which can be extendable. For example, I can connect 6 boards by connecting the I2C lines and power lines together to expand the port number in the system. However, I only want to install the host launchpad to on of the boards which means the I2C line from the last board to the host launchpad could be very long(60 inches). I am looking for some I2C devices to protect the data. Is TCA9509 the right device for this application? Thanks.
Best regards,
Penny