This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS32: absolute maximum rating

Part Number: SN65LVDS32

  • We have been using the  SN65LVDS32D and are considering this device  for other new product design

  • In our current new  design we  have  36 chips of SN65LVDS32D connected in parallel to VCC (pin 16)
    and operating at  -0.7Volt consuming maximum current of 15 mA for duration of 6 hour.
    While the absolute maximum rating  of  the VCC pin as specified in datasheet is   -0.5Volt.

  • Assuming this is a small violation so the voltage deviation can be tolerated as this voltage is applied
     for limited current as low as 15mA.

  • Can we ask to have your reference ? Having Texas Instruments confirmation we may proceed using them
    in our new product design

  • Looking forward to have this request confirmed by TI …We appreciate your efforts…thanks for the fast reply