Part Number: TMDS181
Hi Sirs,
As title, could you help double confirm our schematic if we missed anything.
Thanks!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDS181
Hi Sirs,
As title, could you help double confirm our schematic if we missed anything.
Thanks!!
Hi Sirs,
Sorry for my late reply, Please refer as below
Can you confirm in which mode are you configuring the TMDS181?
A: DP3_TX0~DP3_TX3 are HDMI, CH2 is CLK. Like Table 47
Can you confirm the capacitors value on lanes?
A: 104P/16V
Will you have TMDS AC-coupled on the output? if not, this connection is not necessary (pull up resistors and AC-capacitors).
A: TMDS181 input is from CPU directly connected Cap
We recommend using a 7.06 k resistor at Vsadj.
A:OK
We recommend starting with .2uF on OE pin and remove the pull-up resistor, the TMDS181 has an internal pull-up and populate this capacitor.
A:OK
If you will use the device in sink mode, we recommend using 47k pull-up resistors.
A:OK
Can you confirm the bypass capacitors value? we recommend one 100nF cap on each power pin (Vcc = 3.3V x2, Vdd 1.1V x5), 4.7pF and 10pF on each power node, one bulky cap per power node.
A: VCC and VDD will use 104P, We would like to know 1V2_INC is still need these Cap?
Schematic update as below
If still have some risk on our design please kindly let us know.
Thanks!!