Part Number: TIC12400
Hi Team,
I have a questions about TIC12400.
I think TIC12400 is dsigned for Automotive but my customer want to use it for Industrial PNP/NPN input.
Actually supply voltage in Industrial is 24V typ.
My Question is
"Can TIC12400 support continuous 35Vs(power supply) and also continuous 35VINx(IN0 to IN23 input voltage)?"
if "YES", all spec of electrical characteristics are also covered by continuous 35V?
TIC12400"Q-1" datasheet mentions that recommended operating conditions is 35V but 35V is tested under "table 61" condition.
in customer use-case, power supply is not battery but continuous 24V.
I attached material which shows what customer wants to do.(resistor/ Vth/ current values are just example, no including RIN,COMP)
If There are something worng, could you let me know or if you have any good materials which explan how to use TIC12400 in Industrial, could you share with me?
Thanks,
Regards,
Kai