Part Number: SN65LVDS301
Other Parts Discussed in Thread: SN65LVDS93
Hi team,
my customer is evaluating the SN65LVDS301. Their issue is that the CPU has a I/O level of 3.3V, which is working without an issue, but the datasheet states that the maximum voltage is VDD, in this case 1.8V.
Do you see an issue? Is it okay if the input current is e.g. limited?
In case you see an issue, can you recommend an alternative with 3.3V I/O?
Thank you and kind regards,
Felix