Part Number: PCA9515B
Other Parts Discussed in Thread: TCA9517
Hi
Our customer would like to connect this device to TCA9617 directly. Because PCA9515B is used on the re-used board and TCA9517 is used on new board.
They connects that two board which are the re-used board and new board with I2C. The re-used board can not be redesigned.
On the other hands, it is not allowed if the two PCA9515B is connected in series. (This is mentioned on the datasheet at page 8.)
Is it possible to connect PCA9515B and TCA9617 directly?
Regards,
Koji Hamamoto