Part Number: TUSB1046EVM
Other Parts Discussed in Thread: TPS65982, HD3SS460
Hi~
I want to test with the TUSB1046EVM.
I want to control the TPS65982 PD chip that is configured on the TUSB1046EVM board.
If I look at the TPS6598x configuration tool, it seems that there is no item associated with
the TUSB1046. Is it possible to program change and test with this GUI?
Applying flash of TUSB1046EVM to HD3SS460 + TPS65982 does not seem to operate.
//-------------------------------------------------------------------------------------------
Here is what I want to test.
1. I want to create a device that receives a displayport source and connects to a USB Type C
monitor to test the screen output and data transmission. Add to test is the power test.
2. I want to freely change the voltage og the Vbus output from the monitor to a level
between 5 ~ 20V.
Q. Controlling the TUSB1046EVM from the GUI is not easy, Is is possible to set the power by
changing the set value of Flash Address and Data?
If possible, I would appreciate it if you could give me an Adress and a Value that can be changed.
For reference, I will attach a Flash file read from TUSB1046EVM.
8713.TUSB1046EVM_Read_Flash.zip
Q. I will ask you one more. I purchased the TPS65986 + DP EXPANSION Board. I was testing it using the
GUI, but the factory-installed Flash program was deleted. Can you provide me with the default factory
flash file which consists of TPS65986 + DP EXPANSION Board?