In my design I have a TUSB320LAI that is configured as a UFP and used with a USB port solely for sinking power. On this port there is no USB communication implemented and the only signals I am connecting to is the CC and the VBUS. As far as I understand the TUSB320LAI is compatible with USB 2.0 ports right ? For USB 2.0 there are some host ports that will only provide 100mA until enumeration is established. Thus in my situation \ configuration how is this enumeration accomplished with the TUSB320LAI and will I be limited to 100mA for these types of Hosts ?