Part Number: TSB41BA3B
Other Parts Discussed in Thread: TSB81BA3E
For TSB41BA3, can a single-ended 1.8V oscillator be used instead of a crystal? And if the answer is yes, should the XO pin be terminated? The datasheet describes the XI pin as 1.8V CMOS input, which appears to suggest it is possible.
The reason for the question is that we have a custom TSB81BA3E board laid out for single-ended oscillator, and it looks like TSB41BA3 is mostly pin compatible. We need to support S200b input and trying to avoid board re-layout. Thank you.