Part Number: DS90UB947-Q1
Hi,
I got some questions about this devices related to the pixel speed and position as follows:
-
Can you confirm that in “Single-Pixel” mode minimum frequency for pixel_clock is 25MHz and in “Dual-Pixel” mode is 50MHz, that is equivalent to a minimum frequency of 25MHz on LVDS_PCLK (2 pixel per clock period)?
-
Is it possible to use “Dual-Pixel” mode if FPD-Link III interface is set as SINGLE-LANE (the receiver has a single LANE)?
-
We do not understand bits mapping as reported in Figure 15 and Figure 16 of datasheet. If serializer generates stream video with mapping as in Figure 15, we have to set bit[7] of register 0x4F at ‘1’ (SPWG mapping) to have correct visualization. Otherwise with mapping as in Figure 16, bit[7] of register 0x4F should be at ‘0’ (OpenLDI mapping). The figures seems to be reversed.Can you verify?
Thanks
Umberto