Part Number: SN65DP159
Other Parts Discussed in Thread: TMDS181
Team,
Could you please answer my customer question.
I have a short question regarding to the SN65DP159. The chip (and also the DP159) has internal 50 ohm pullups for the input signals (IN_D[2:0] and IN_CLK). But what is the reason why there are additional external 50 ohm resistors on the evalboard?
Page 24 : http://www.ti.com/lit/ds/symlink/sn65dp159.pdf
Page 12 : http://www.ti.com/lit/ug/sllu225/sllu225.pdf
I added them also in my schematics, but now I don't want to create stubs with vias to connect the resistors, which are normally not needed.
Thank you in advance.
-Needhu