Part Number: TSU6721
Dear TI
I used the muic : TSU6721 for my project.
After software retset (set BIT0 of 1Bh Reg) I try to enable interrupt by set bit INT MASK of 02h Reg to 0.
After that plug in the USB cable. I disable interrupt and read 05h and 06h Reg, The values of both regs always are 0.
As my understand the CONNECT (bit 5) in 06h Reg should be high as referring to TSU6721EVM user's guide.
I hope to receive some suggestions about proper configuration or procedure in order to make interrupt or interrupt mask
Thank you so much !