Part Number: DP83822IF
Hi all
Would you mind if we ask DP83822IF?
We are so sorry to keep bothering you.
We would like to understand about Table 12. LED_0 Configuration on the datasheet P47 correctly.
ON for Good Link -> Does it mean that the condition is good link?((Address0x01's b2 Link status is 1 = Valid link established (for either 10 Mbps or 100 Mbps operation), right?)
OFF for No Link -> Does it mean that the condition is link loss?(Address0x01's b2 Link status is 0 = Link not established, right?)
Will LED_LINK deassert in accordance with the Link Loss Timer as specified in the IEEE 802.3 specification?
Kind regards,
Hirotaka Matsumoto