This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS100MB203: Is thie part capable of operating at lower data rates

Part Number: DS100MB203


Hello team,

Please see below customer question:

Is this part capable of operating at lower datarates? 

It says up to 10.3125Gbps, but I can’t find if there is a low end of the operating range. 

If possible, we would like to use it as a mux for an SFP+ module, but we need that interface to also operate with a lower speed 1Gbps SFP module.

Regards,
Randhir