Hello,
I am using a product/device that uses TUSB3410 driver to communicate.
I install TI driver that comes along with the product and it was working fine few days.
Recently I did few installation and un-installation of TI driver which caused some issue and currently I am not able to communicate with the device. During my analysis of the problem I found that, when I connect the device to my PC TI driver is installed/showing in two different place under device manager ie., under "Multi-port serial adapters" and also under "Ports (COM & LPT)". In both the place TI driver is showing the version as 6.6.2000.0
I am using Windows 7 in my PC. Since the device was working fine earlier I don't think this could be some windows 7 issue. I believe something got messed-up when I try to uninstall and reinstalling the driver.
Could anyone please help me in fixing this issue?
Thanks
Suresh Kumar Ramu