Part Number: DS90UB964-Q1
[ DS90UB964-Q1 ] MAX_FRM_HI & MAX_FRM_LO Register
Hi,
Let me confirm the function of "MAX_FRM_HI" and "MAX_FRM_LO" registers.
The 16bits frame counter is consist of these two registers.
if both registers are not set to "0", this can count up to 65535.
However, for example, MAX_FRM_HI is set to "0" and MAX_FRM_LO is set to "1",
in this case, the maximum frame count is limited to 255.
Correct?

Thanks,
Ken